GridColour

The GridColour defines the color of the grid lines on an embedded List. You can animate this so that it uses a color that is associated with a database item (such as the alarm color), refers to a custom color, or is set to a specific color (an RGB value).

This property works in a similar way to the FillColour except that it applies to the grid lines of an embedded List instead of the fill of an object.