Mimic Editing Features

When you have added objects to a Mimic, you will need to edit them so that they are the appropriate size and color and use suitable fonts, animations, pick actions, and so on.

To alter the color and configuration of a Mimic object, you need to access its Properties settings. To do this, you need to display the object's Properties window. You can also use the Properties window to set up animations and pick actions. For more information, refer to the Editing section that applies to the object you want to configure. For example, if you want to change the color of a pipe, refer to the Editing a Pipe section.

Each Mimic object also has an editing pick menu. You can access the editing pick menu by right-clicking on the required object (in Design mode).

The editing pick menu has the following options which you can use during the design of your Mimic:

There are also useful Mimic editing features available via the Graphics Tab on the ViewX ribbon.