Configure the Mitsubishi Point Properties

Use the fields at the top of the Mitsubishi tab to configure the Mitsubishi-specific point properties. Some of these properties are common to points on many simple drivers—for information, see Configure Common Point Properties in the Geo SCADA Expert Guide to Simple Drivers. Properties that are specific to analog points on the Mitsubishi driver are explained below.

If the Word Offset and Data Type are inappropriate, a diagnostic message is generated.

Example 1:

An analog value has a DINT data type, and is located at addresses 16 to 17 within a block of scanned data in a PLC. The Words are not swapped.

The present value of the analog is:

Word 16 = 1
Word 17 = 0

As the Words are not swapped, this results in the analog point being given a value of 1 within Geo SCADA Expert.

If the configuration was such that the Words were swapped, this would result in the analog point being given a value of 65536 within Geo SCADA Expert.

Example 2:

A DOUBLE (64-bit double precision floating point) obtains its data from the Mitsubishi Link Registers W030A to W030D.

The registers are not swapped, therefore register W030D contains the most significant Word.

(If the registers were swapped, register W030A would contain the most significant Word, and register W030D the least significant.)