Configure the Modbus Point Properties

Use the fields at the top of the Modbus tab to configure the Modbus-specific point properties. Some of these fields are common to many simple drivers (see Configure Common Point Properties in the Geo SCADA Expert Guide to Simple Drivers). Fields that are specific to the Simple Modbus driver are explained below: