Configure the Scanner Properties

Use the fields on the Scanner tab to define the driver-specific properties for a scanner. Some of these fields are common to many scanners—see Define Common Scanner Properties in the Geo SCADA Expert Guide to Simple Drivers for information. Those fields that are specific to scanners on the Simple Modbus driver are described below.

Use the fields on the tab to: