Configure a Modbus Slave Channel’s TCP/IP Connection Properties

For a Modbus Slave channel to communicate using Modbus Transmission Control Protocol (TCP), set the channel’s Connection Type to TCP/IP.

Use the rest of the fields on the Connection tab to define the required connection properties: