Minimum Configuration

For an ODBC Connection to become functional (online), you need to:

You also need to put the connection In Service and save the configuration.

These are the minimum requirements and, when defined, will result in a functional connection that uses the default configuration settings.

ATTENTION: An ODBC connection can be affected by factors other than the configuration parameters within ViewX, which can cause the database to lock and stop data from being recorded