Configure the Scanner Properties

Use the fields on the Scanner tab to define the driver-specific properties of a scanner. Many of these fields are common to various scanners (see Configuring Scanners on Simple Drivers in the Geo SCADA Expert Guide to Simple Drivers). Those fields that are specific to scanners on the Simple OPC driver are described below.