Configuring String Points

Use Simple OPC String points to map text strings on OPC servers into Geo SCADA Expert.

Configure the properties of each String point using the fields on the Simple OPC String Point Form.

For information the String Point tab on the String Point Form, see Defining String Point Details in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the Control tab, see Define the Control Settings for a String Point in the Geo SCADA Expert Guide to Core Point Configuration.

For information on the fields on the OPC tab, see Configure General Properties on the OPC Tab, and see Specify the Source Value of a Point.

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers.