Configure the Queue Parameters

The <Point Type> tab on the Forms of OPC UA Analog, Digital, String and Time points contains a Queue Parameters section. You use the properties in this section to define the queue parameters.

The Queue Parameters section contains the following properties: