Connection State Alarm

Associated with: OPC UA Servers

This status attribute indicates the state of the connection between the OPC UA server and Geo SCADA Expert.

Possible states: Displays one of the Standard Alarm States.

If this attribute indicates that Geo SCADA Expert has detected a problem, look at other status attributes and Event Journal messages to help ascertain the cause.

Also see Connection State.