Introduction to the OPC XML-DA Client Driver

This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is designed for use by engineers who are responsible for configuring OPC XML-DA Client-specific items and features. It can also be used by system administrators when investigating any unexpected behavior relating to the OPC XML-DA Client.

Document Scope

This guide explains how to configure OPC XML-DA Client specific features and items in the Geo SCADA Expert database. It also describes how to use the OPC XML-DA Client specific statistics and diagnostics.

The OPC standards are a series of standard specifications aimed at allowing inter operability between different SCADA systems. Geo SCADA Expert uses these standards to allow transfer of data between the Geo SCADA Expert server and third-party applications.

The OPC eXtensible Markup Language Data Access (XML-DA) standard is specifically aimed at facilitating the transmission of plant data over the internet (see Which Driver?).

Geo SCADA Expert’s OPC XML-DA Client driver is used to read and/or write to data on XML-DA servers, including Geo SCADA Expert or third-party servers, using the OPC XML-DA protocol. The driver enables Geo SCADA Expert to communicate with servers that comply with OPC XML-DA version 1 or 2. The driver takes into account any security settings, designed to limit access to configuration properties on many OPC servers.

The OPC XML-DA documentation explains how to configure OPC XML-DA specific features and items within the Geo SCADA Expert database (see Configuring OPC XML-DA Devices in Geo SCADA Expert).

It also explains driver-specific aspects that may be of interest to system administrators and engineers when investigating unexpected system behavior (relating to the OPC XML-DA Driver). For more information, see OPC XML-DA Specific Status Display Attributes, and see OPC XML-DA Specific Driver Log File Options.

NOTE: There are no driver-specific pick actions for database items on this particular driver. However, users with the required privileges can add custom pick actions to a database item by using the User Methods tab on the relevant configuration Form (see Using the User Methods Tab to Define Custom Actions in the Geo SCADA Expert Guide to Core Configuration). See a system administrator for the documentation associated with such custom actions (also known as ‘methods’).

Policy of Continuous Development

To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).

Further Information

OPC Foundation Standards: see www.opcfoundation.org