Configure Point Scaling

Use the fields within the Scaling section of the Analog Point tab to configure the scaling of a point. Geo SCADA Expert applies scaling to each value that it receives from the device. This is in addition to any scaling that takes place at the device (see Configure SCADAPack 50 Device Point Properties).