Firmware Type
Associated with: SCADAPack controllers
This attribute indicates the type of firmware that is running on a controller. The attribute is displayed once a controller is or has been in communication with the server.
Telepace
(for a controller that is running Telepace firmware)