Configure Modbus Server Device General Settings

When you create a Modbus Server Device item you need to configure the following general settings to identify the Server Device and associate it with the SCADAPack x70.

In Service

Use the check box to specify whether the Modbus Server Device is 'In Service' and included in the downloaded/exported configuration (see The 'In Service' Check Box and Items Taken Out of Service).

If you take a Modbus Server Device out of service, its Modbus Point Scanners become out of service (although their configuration remains unchanged).

SCADPack x70 Device Configuration

Use the field to enter the name of the SCADAPack x70 Device Configuration device that this server device is associated with. Use the browse button to display a Reference browse window and then select the required entry from the window.

Device Name

Enter a suitable name for the item taking into account the following restrictions:

  • Maximum length is 14 characters
  • The first character must be alphanumeric
  • Subsequent characters must be alphanumeric or an underscore.