Configure a Modbus Server Device

You have to create a separate configuration item for each Modbus Server Device that you want SCADAPack x70 to scan. A SCADAPack x70 Modbus Server Device configuration item enables you to configure and store the configuration settings on the SCADAPack x70 device. When you have created a Modbus Server Device item, use the Modbus tab to configure the settings.

You can add a maximum of 150 Modbus Server Devices to a SCADAPack x70 device.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.