File
Associated with: SCADAPack x70 Firmware Image items
This status attribute indicates the name of the binary firmware image file that was last imported into the Geo SCADA Expert database using this particular Firmware Image item (see Import Firmware Image). The date and time of the last import process is included.
Use this status attribute in conjunction with the Description attribute to ascertain information about the .biz file with which this particular Firmware Image item is associated.
"911e57x.biz" Modified at 2025-05-29 10:05:32