Port Function - PPP/TCPIP

This port is used for TCP/IP communications. The port can be used for any enabled TCP/IP Service and DNP3. If this port Function is selected, you need to enable and Configure TCP/IP Services.