SCADAPack Import File n

Associated with: SCADAPack x70 Device Configuration items

You can use the Import from RemoteConnect pick action to import SCADAPack Import configuration files into Geo SCADA Expert from SCADAPack RemoteConnect software. You can use the Upload Configuration pick action to upload the configuration from the SCADAPack x70 device into Geo SCADA Expert.

The SCADAPack Import File n status attributes indicate the files that are included in the last SCADAPack Import configuration file to be imported or uploaded into Geo SCADA Expert for the selected SCADAPack x70 Device Configuration item. There is one SCADAPack Import File status attribute per separate file in the SCADAPack Import. Each SCADAPack Import File status attribute is assigned a different number.

 

SCADAPack Import File 1 "configuration.rtu"

SCADAPack Import File 2 "station.apx"

SCADAPack Import File 3 "logicapp1.sta"

SCADAPack Import File 4 "logicapp1.sig"


The SCADAPack Import File n status attributes for an imported or uploaded SCADAPack Import configuration file that contains the 4 files that are listed in double quotation marks above.

For further information about the imported or uploaded SCADAPack Import configuration file, use the SCADAPack Import File n status attribute(s) in conjunction with the Device Configuration item's SCADAPack Import status attribute.

SCADAPack Import File n status attributes are only displayed if a SCADAPack Import configuration file has been imported or uploaded into Geo SCADA Expert for the selected SCADAPack x70 Device Configuration item.

Further Information

For information about the types of file that might be included in a SCADAPack Import configuration file, see the documentation provided with the SCADAPack RemoteConnect software.