Set up the Application Layer

The Application Layer is the highest user-configurable DNP3 communication level. Use the following fields within the Application Layer Setup section of the DNP3 Settings tab to specify the properties of the SCADAPack x70 device’s application layer:

Application Layer Attempts

Specify the number of times that the SCADAPack x70 device will send any Application Layer Fragments. Fragments are re-sent if an Application Layer Confirm for the fragment is not received within the Complete Fragment Timeout.

This field specifies the number of Attempts, not the number of Retries.

Application Layer Timeout

Specify the time (in seconds) within which the outstation requires a response to peer application layer requests. If no response is received within this time, the outstation re-sends the request fragment. This sequence is repeated until either a response is received, or the number of attempts equals the number specified in the Application Layer Attempts field.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

File Inactivity Timeout

This allows you to specify (in seconds) the outstation file inactivity Application layer timeout. If a file transfer operation is in progress (for example, if a file is open) this is the maximum amount of time allowed between operations. If no file transfer operations occur in this period the file is closed and future file transfer operations on this file will fail. The timer restarts after each successful file transfer. The time specified needs to be sufficiently long enough for the expected upload / download file sizes and the speed of the communications link(s). The valid range is from 5 seconds to 3600 seconds. The default is 120 seconds.

Select Arm Timeout

Specify the time period (in seconds) within which the outstation has to receive an Operate command after receiving a Select command for a two-phase Select / Operate DNP3 Control. The valid range is 0 to 65 seconds. The default is 10 seconds.

If the Operate command that corresponds to the Select command is received before the timeout elapses, the outstation performs the control operation.

If the Operate command is not received within the specified time period, the control operation is rejected.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

Default Pulse Time

Specify the duration, in milliseconds, of the activation time of a pulse of a digital object state, when the initiator of a pulse operation does not provide a pulse time. The valid range is from 0 milliseconds to 65535 milliseconds (inclusive). The default value is 250 milliseconds.

The SCADAPack x70 device uses the Default Pulse Time when you:

  • Control a SCADAPack x70 DNP3 Pulse Action (NULL), when the On Time field on the NULL tab is set to 0 (see Configure a NULL Pulse Action).
  • Control a SCADAPack x70 DNP3 Pulse Action (Trip-Close) when the On Time fields on the Trip/Close tab are set to 0 (see Configure Trip and Close Pulse Actions).
  • Use Inching to control a SCADAPack x70 DNP3 Pulse Action (NULL) or a SCADAPack x70 DNP3 Pulse Action (Trip-Close) when the On Time field is set to 0.
  • Control a SCADAPack x70 DNP3 Binary Output point that is associated with a SCADAPack x70 Digital Configuration item where the DNP3 Static Group and Variation is set to either Binary Output Trip (g12) or Binary Output Close (g12) (see Specify the DNP3 Static Group and Variation).

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

Time Update Request Rate

Specify how often the outstation requests a time update from its DNP3 Master (Geo SCADA Expert). The request is sent as a DNP3 IIN bit set in responses sent to the Master.

Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value.

Maximum Transmit Fragment Size

A SCADAPack x70 device sends messages in fragments, which contain one or more frames. A frame is a variable-size data packet. Use this field to specify the maximum size of a fragment sent by the outstation. The fragment's size is determined by the SCADAPack x70 device's buffer. In environments with high levels of interference, reducing the fragment size may alleviate communications problems.

The size is determined by the receiving device’s buffer and the network type:

  • Serial ports: 100 to 2048 bytes
  • Ethernet ports: 254 to 2048 bytes
  • USB ports: 1000 bytes

Messages that are larger than one fragment are sent using multiple fragments. Large fragments and multiple fragments are transmitted using more than one frame (for instance, a fragment of 2048 bytes needs breaking into at least 9 frames). Where this occurs, the frames are reassembled into the complete application fragment by the receiving device.

Security Reply Timeout

This allows you to specify (in milliseconds) the Secure Authentication reply time for outstation messages. The valid range is from 100 to 360,000 milliseconds and the default is 2000 milliseconds.

Default DNP3 Transport

Use the combo box to specify the default transport protocol that is to be used to transmit outbound (initiating) DNP3 frames across LAN/WAN links. Response frames use the same protocol as the initiating frames. Choose from:

  • TCP—Use Transmission Control Protocol (TCP), a connection-orientated transport protocol
  • UDP—Use User Datagram Protocol (UDP), a connection-less transport protocol.

    This is the default setting.

If the SCADAPack x70 device is an end node in a TCP/IP network and DNP3 communications are used, use the same setting as the DNP3 Master Transport, unless the DNP3 Routing Table Connect Number property overrides this.

Default DNP3 Port

Specify the TCP/UDP port number to which DNP3 frames are sent and from which they are received. The valid range is from 0 to 65535 (inclusive). The default is 20000, which is the IETF assigned port number used by the DNP3 protocol.