Minimum Configuration

For a SNMP point to be capable of functioning, as a minimum you have to specify these features on the <Point Type> tab:

If you want point data to be stored historically, you also need to:

Also ensure that the point is In Service, and has saved, valid configuration. This will produce a point that is capable of functioning using the default configuration settings.

Note: For SNMPv2 and SNMPv3, points must be linked to a SNMP device. If you require SNMPv3 security you will need to create and configure an SNMP Device and associate the point(s) with the device.

see Create an SNMP Device