App.Head

The App.Head property is an application property. You can use the property to return the head number that is assigned to the Window Container in which the script is running (see Assign a Head Number to a Window Container in the Geo SCADA Expert Guide to Client Administration). This is only of any practical use on a Multi-Monitor setup.

The App.Head property is only for use in Mimic Scripts.

When the App.Head property is used in a Mimic script:

Syntax

App.Head

Description

Returns the head number that is assigned to the Window Container in which the script is running.

Arguments

None

Returns

Integer. This can be:

0 - For a Virtual ViewX Client. Virtual ViewX clients return 0, even if there are multiple browser windows open.

1—10 - The script is running in the Window Container that has the returned value assigned to it as a head number.

Example:

In this example, the script will cause a Virtual ViewX Client to navigate back to the previous page. However, the same script will cause a ViewX client to close the Mimic instead.

IF App.Head =0 THEN

Mimic.GoBack()

ELSE

Mimic.Close

END IF

Further Information

Embedded Mimics: see Embed a Mimic on a Mimic in the Geo SCADA Expert Guide to Mimics.

Shared with Other Embedded Mimics Property.