Application Functions and Properties

The Application script object ('App') has functions and properties that affect ViewX. They allow a script to perform various tasks in ViewX, including opening windows, logging on and off, changing a password, displaying the online help, exiting ViewX and returning the head number assigned to the Window Container on which the script is running.

Unless stated otherwise, you can use the Application object and its functions and properties in both Mimic and Alarm Banner scripts.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.