ServerQuery.RowCount
The ServerQuery.RowCount property returns the total number of rows in the Query that is returned by the Server.Query property.
| Syntax |
ServerQuery.RowCount |
| Description |
Returns the total number of rows in the SQL Query that is returned by the Server.Query property (see Server.Query). |
| Arguments |
None. |
| Returns |
Count {integer}. The count is the total number of rows in the Query that is returned by the Server.Query property. |
For an example that shows how the ServerQuery.RowCount property can be used, please refer to Server.Query.