Learn about the Driver Request Timeout settings. Learn about the Scanner Timeout settings. Learn about the PSTN Eavesdropping Timeout setting. Learn about the settings in the Driver Start and Stop Timeouts section. Learn about the Maximum Clock Jump setting. Learn about the Control Feedback Grace Period. Learn about the Asynchronous Point settings. Learn about the Value Map Scanning Interval. Learn about the Server Poll Interval. Learn about the On Demand Direct Outstation Retry Period. Learn about the Maximum Batch Size for Server Updates. Learn about the Queue Request setting. Learn about the settings in the Resolve Host Names section.

Driver Settings

You can use the Drivers section of the Geo SCADA Expert Server Configuration Tool to:

Before you define the various timeout, update, and interval settings, we recommend that you familiarize yourself with the information in Understanding Request Timeouts.

For information on the various driver specific sections of the Geo SCADA Expert Server Configuration Tool, such as Crystal Reports and DNP3, please refer to the relevant driver guide.