Historic Configuration Settings

You can use the Geo SCADA Expert Server Configuration Tool to define various historic settings that are applied to the entire system. The historic settings allow you to configure many historic features including:

The Historic Configuration branch allows you to define the settings for a variety of features relating to the storage of historic data. The settings for each of the Historic / Event Journal / Configuration Change features are organized into the following groups (which you can access via the Server Status Tool’s hierarchy):

Further Information

Historic Views.