Importing Historic Data

Geo SCADA Expert allows you to import historic data into point and accumulator histories using a set of Historic aggregate methods. The method you use depends on the amount of data that you want to import or insert into the database.

LoadDataValue

This method allows you to import a single value to any point in your database.

Format:

LoadDataValue ( Reason{Byte}, Quality{Long}, Time Stamp{Time}, Value{Variant} )

1

The following code illustrates a Visual Basic use of this method to import a single value to a single point using Server Automation:

Dim objServer = New ScxV6DbClient.ScxV6Server

objServer.Connect("system name", "username", "pwd")

Dim obj = objServer.FindObject("Array Group.AG01")

Dim His = obj.Aggregate("Historic")

His.Interface.LoadDataValue(1, 192, #7/3/2016 5:22:23 PM#, 13)

 

obj = Nothing

objServer.Disconnect()

2

The following code (written using VBScript) illustrates the same example code used as a script within ViewX:

sub ImportValue()

Set obj = Server.FindObject("Array Group.AG01")

Set His = obj.Interface.Historic

His.LoadDataValue 1, 192, #7/3/2016 5:22:23 PM#, 13

end sub

LoadDataValues

This method allows you to import an array of values to any point in your database.

Format:

LoadDataValues ( Value{Array of Variant}, Time Stamp{Array of Time}, Quality{Array of Long}, Reason{Array of Byte} )

A separate array needs to be created for each parameter within the method.

1

The following code illustrates a Visual Basic use of this method to import an array of five values to a single point using Server Automation:

Sub Main()

Dim Svr As ScxV6DbClient.ScxV6Server

 

Svr = New ScxV6DbClient.ScxV6Server

Svr.Connect("system name", "username", "pwd")

Dim obj = Svr.FindObject("Array Importing.AG01")

If obj Is Nothing Then

REM Object not found

Exit Sub

End If

 

REM object found

Dim His = obj.Interface.Historic

If His Is Nothing Then

REM Object does not have Historic aggregate, not Historic enabled

Exit Sub

End If

 

Dim PointValues = New Double() {13, 14, 15, 16, 17}

Dim PointTimeStamps = New Date() {#2016-07-03 16:23:23#, #2016-07-02 16:24:23#, #2016-07-02 16:25:23#, #2016-07-02 16:26:23#, #2016-07-02 16:27:23#}

Dim PointQuality = New Integer() {192, 192, 192, 192, 192}

Dim PointReason = New Byte() {1, 2, 3, 4, 5}

 

His.LoadDataValues(PointValues, PointTimeStamps, PointQuality, PointReason)

 

obj = Nothing

Svr.Disconnect()

End Sub

2

The following code (written using VBScript) illustrates the same example code used as a script within ViewX:

sub ImportValues()

Set obj = Server.FindObject("Array Importing.AG02")

Set His = obj.Interface.Historic

Dim PointValues

Dim PointTimeStamps

Dim PointQuality

Dim PointReason

 

PointValues=Array(13, 14, 15, 16, 17)

PointTimeStamps=Array(#7/3/2016 4:23:23 PM#, #7/3/2016 4:24:23 PM#, #7/3/2016 4:25:23 PM#, #7/3/2016 4:26:23 PM#, #7/3/2016 4:27:23 PM#)

PointQuality=Array(192, 192, 192, 192, 192)

PointReason=Array(1, 2, 3, 4, 5)

 

His.LoadDataValues PointValues, PointTimeStamps, PointQuality, PointReason

 

end sub

The 'Reason' parameter is optional. If this parameter is omitted it defaults to 0 (Current Data).

A maximum of 5,165 elements are allowed in the arrays, an error is raised if this number is exceeded.

LoadDataValuesEx

This method allows you to import an extended version of the historic properties as an array of values to any point in your database. The method follows a similar format to LoadDataValues.

Format:

LoadDataValuesEx ( Value{Array of Variant}, Time Stamp{Array of Time}, Quality{Array of Long}, Status{Array of Long}, State{Array of Byte}, Reason{Array of Byte}, MSState{Array of Byte} )

The Status, State, Reason and MSState parameters are all optional.

The Status parameter is a bit mask of flags that varies between drivers.

To calculate the State from the Value specify the state as 255 (or omit the parameter).

If there is no master-station state (or the feature is disabled) then specify the MSState as 255 (or omit the parameter). (For more information about master station state, see Master Station Alarm Limits in the Geo SCADA Expert Guide to Core Point Configuration.)

LoadDataFile

This method allows you to use a datafile as a source to import historic data for one or more objects in the database. This method does not have the same restrictions on the amount of data as the LoadDataValues method and is also much faster at loading the data.

Format:

LoadDataFile ( Filename{String} )

It is recommend that you use a CSV file as a file format for importing the data. When creating the file, be aware of the following:

  • Store the CSV file on the Geo SCADA Expert server that is currently running as the Main server. This requirement applies even if you intend importing the data using VBScript that is running on a Mimic on a client.
  • Ensure that each line of the CSV file specifies a single record and has the format:

    YYYY,MM,DD,HH,MM,SS,Value[,Quality]

    (where 'Quality' is optional (see below))

    1

    The following code illustrates a Visual Basic use of this method to import a file using Server Automation:

    Sub Main()

    Dim Svr As ScxV6DbClient.ScxV6Server

     

    Svr = New ScxV6DbClient.ScxV6Server

    Svr.Connect("system name", "username", "pwd")

    Dim obj = Svr.FindObject("Array Importing.AG01")

    If obj Is Nothing Then

    REM Object not found

    Exit Sub

    End If

     

    REM object found

    Dim His = obj.Interface.Historic

    If His Is Nothing Then

    REM Object does not have Historic aggregate, not Historic enabled

    Exit Sub

    End If

     

    His.LoadDataFile("D:\AG01HistoricTest1.csv")

     

    obj = Nothing

    Server.Disconnect()

    End Sub

    2

    The following code (written using VBScript) illustrates the same example code. However, in this case, it is used as a script within ViewX to import historic data for a single point:

    sub AddDataFileAG03()

    Set obj = Server.FindObject("Array Group.AG03")

    Set His = obj.Interface.Historic

    His.LoadDataFile "D:\AG03HistoricTest.csv"

    end sub

    The data format within the file should be similar to the following:

    2016,07,03,16,23,23,0

    2016,07,03,16,24,23,12

  • The file must use the ANSI encoding format. Other encoding formats will cause the import to fail.
  • The 'State' (and 'MS State' if the Master Station Alarm Limits feature is enabled) of each historic record are calculated automatically.
  • The 'Reason For Logging' for each historic record is fixed as 0 ('Current Data').
  • The 'Quality' for each historic record is optional. If the 'Quality' element is omitted, the 'Quality' of the historic record defaults to 192 ('Good'). For example:
    2016,07,03,16,25,23,15.2,192.