Protect the Permanent Standby Servers

Geo SCADA Expert allows you to increase the Keep online for setting to extend the period of historic data synchronized from the Main server to Permanent Standby servers. The Protect Permanent Standby Servers when increasing online period feature allows you to ensure that the existing data on Permanent Standby servers is not deleted when you extend the period. By default Permanent Standby servers are protected when you increase the Keep online for period on the Main.

This applies to Event Journal and Configuration Changes as well.

There are occasions when the protection of permanent servers should be removed, for example, when restoring or rebuilding a Main server, see Specify the Duration to Retain Historic Data Online. The following sections illustrate the effect of this feature and how Historic data is affected.