Set the Type of Server

The Server Configuration Tool’s System Configuration>Partners settings include Type, which you can use to define the type of server architecture to which the server you are configuring belongs. For example, if you are configuring a server that is to be a Standby server in a Triple Standby architecture, you should set the Type to Triple Standby.

The Type setting defines the server’s role in the system architecture and can be set to:

WARNING

COMPLETE LOSS OF CONFIGURATION

When setting up a main-standby system, make sure that you restart the servers in the correct order if objects are already configured in your database. Make sure that the server with objects already configured is started first and is running as main, then start the partner servers and allow them to synchronize with the main server.
Failure to follow these instructions can result in death, serious injury, or equipment damage. Failure to start the servers in the correct order can result in the complete loss of configuration from the system, requiring recovery from a backup.