Using a Registry Editor to Change Server Log File Settings

You can use a Registry Editor such as Regedit to make changes to the log file settings (such as maximum number of files, location of files, and so on). For some applications, such as port server, the only way to alter the log file settings is to use a Registry Editor.

To change the log file settings:

  1. Access and Run a Registry Editor.
  2. Use the Registry Editor to locate the registry settings at the relevant location.

    The default locations are as follows:

  3. Define the registry settings:
    1. Right-click on a setting to display a context sensitive menu. The settings include:
      • LogEnable—Enter True, Yes, T, Y, or 1 to enable logging or enter False, No, F, N, or 0 to disable logging as required.
      • LogFileBase—Define the folder that will contain the log files and the filename prefix for the files. The prefix is the name of the files (it cannot contain certain characters, see your operating system documentation for more details).
      • LogMaxFiles—Enter the maximum amount of log files permitted for each set of log files. When a new log file is created, the oldest log file is deleted (to make way for the new file).
      • LogMaxSize—Enter the largest size of a log file. The size is in kilobytes.

        The actual file size is likely to exceed the size that is specified in this field. This is because the server completes writing the full line of log entries before the file size is checked.

      • LogOldFiles—Enter the number of sets of log files that can be stored for each instance of an application.

        For many systems, the default setting of 1 is adequate.

    2. Select the Modify option to display the Edit window.
    3. Enter the required setting in the Value Data field (see step i for the required settings).
    4. Select the OK button to confirm the setting.
    5. Repeat the sub-procedure (i-iv) for each logging setting.