Access Documentation for a Specific Driver

Documentation is available for many of the drivers that Geo SCADA Expert supports. For drivers published by Schneider Electric, there is documentation included in the Geo SCADA Expert online help, while other publishers may provide access to other forms of documentation, such as web pages or downloadable PDFs.

If you are using the Sever Status Tool, you can follow these steps to access documentation for a driver:

  1. Display the Modules status information in the Server Status Window (see Modules).
  2. From the list of drivers that are installed, right-click on the driver for which you need help.
  3. Select Help from the context-sensitive menu. This links to the documentation for the driver. If there is no documentation available for the driver, the Help option is not included in the context-sensitive menu.

You can also access the online Help for a driver from a ViewX or Virtual ViewXclient (see Display Geo SCADA Expert Help).