Diagnostics

The Diagnostics category provides statistical information about system activity. You can use this information to investigate the amount of system traffic.

The traffic status information is shown in rows, with each row representing a different type of Statistic. The rows are: