Links (WebX)

The WebX branch of the Server Status Tool includes a Links category. The category provides status information about the connections between the server and any Original WebX clients.

The status information for the Original WebX links is categorized as:

You should pay particular attention to the number of links shown in the Links category, and the Long Time status value.

If the number of links is excessively high in comparison to the number of Original WebX clients (typically, there are between 1 and 3 links per Original WebX client), you should contact Schneider Electric for assistance.

If the Long Time status value is more than 1000mS, there may be a high server load (see Original WebX Client Activity).

Further Information

Original WebX Status Information.