Searches

The Searches category contains information about the current search requests for data in the database. The searches information can be used to help determine the cause of slow client response.

If a client is slow to respond to a search, the cause may be:

The Searches information allows you to determine if the latest search was completed quickly—if so, the search is suitable and the problem is being caused by a lack of resources or a network problem.

By examining the number of searches, you can determine the level of demand being placed on the server or client. If the number of searches is high and many of the searches are taking a long time to complete, there may be a high demand on the available resources. In this situation, we recommend that you contact Schneider Electric.

The Searches category provides the following information for each search: