Database Web Server Connection Problems

You can use the Information category to determine the status of the Database Web Server connection (see General System Status Information). The status for the connection between Geo SCADA Expert and the Original WebX displays the following two messages by default:

The following messages appear when a problem occurs relating to the Database Web Server: