XML-DA Items

The OPC branch of the Server Status Tool includes an XML-DA Items category. The category provides status information about the XML-DA tags to which XML-DA clients are subscribed. Status information is shown for XML-DA tags when XML-DA is used to access the database. Each XML-DA tag represents a path to a value for an item.

The status information for each XML-DA tag is categorized as:

 

Totals

When the XML-DA Items category is populated with entries, a Totals row is added to the bottom of the list of entries.

The Totals row indicates the total number of rows (excluding the Totals row), along with the total Update Count of all of those rows.

 

You can access a context-sensitive menu by right-clicking on an entry in the list. The menu has this option:

If the Reset Counters check box is selected on Server Snapshot Log files, the counts will also be reset whenever a snapshot is taken (see Server Snapshot Log Files in the Geo SCADA Expert Guide to Server Administration).