Configure the Scan Properties

Use these fields on the Scanner tab to define properties such as the scan rate, scan offset, and the type of data that is to be scanned.

You can also specify whether the scan rate is increased whenever any of the associated points are displayed on a client (see Define Whether a Scanner is Promoted While its Points are on Display in the Geo SCADA Expert Guide to Simple Drivers).

For information on fields that are available for many scanners, see Define the Scan Rate in the Geo SCADA Expert Guide to Simple Drivers. Fields that are specific to Simatic S7 scanners are explained below: