Operational Limitations - Client

Geo SCADA Expert has a number of recommended operational limits. Expansion beyond the recommended limits is possible, but may result in a system that is unstable and unreliable. The recommended operational limits for Geo SCADA Expert clients are:

Parameter

Limit

Notes

Minimum ViewX to Geo SCADA Expert server link bandwidth

2 Mbit

Exceeding these limits will cause slow performance in ViewX.

Maximum ViewX to Geo SCADA Expert server link latency

50 ms

Exceeding these limits will cause slow performance in ViewX.

Minimum Virtual ViewX client to Virtual ViewX server link bandwidth

1 Mbit

 
Minimum Original WebX client to Geo SCADA Expert server link bandwidth

2 Mbit

 

While these are recommended operational limits, we do not guarantee performance even if your system is operating at or under these limits. This is because it is possible to configure aspects such as data processing and client displays that are detrimental to performance. We recommend that you review the Design Guidelines and Performance Guidelines online on the Schneider Electric Community website.

You are restricted to having up to a maximum of 5 Geo SCADA Expert displays open simultaneously on a Virtual ViewX client (providing that your User Account provides Multi Document Interface access).

Further Information

Server operational limitations: see Operational Limitations - Geo SCADA Expert Server.