Screen Resolution and Color Depth

The minimum recommended screen resolution for Geo SCADA Expert is 1024x768, with a display that is running in true color (24 bit or 32 bit color depth).

Server class computers and virtual machines (VMs) on server class computers should not be used to run ViewX in a day-to-day operational environment; instead, appropriate client machines should be used. Client machines often have a higher graphics hardware specification than server class computers. This higher graphics specification is required to run ViewX in a day-to-day operational environment, within which users might perform graphics-intensive tasks such as viewing complex Mimics, or working with multiple or floating documents (see Client PC Specifications).

The standard graphics hardware on server class computers and on VMs on server class computers may only be adequate for running ViewX for administrative purposes (such as performing initial system configuration and user account setup).