Configure TBox Alarm Limits

Use the fields within the Alarm Limits section of the TBox Analog Point tab to set limits for a point and specify whether an alarm or event is generated if the point exceeds those limits.

Many of the Alarm Limits fields are common to many analog points (see Configure the Limits for an Analog Point in the Geo SCADA Expert Guide to Core Point Configuration).