Define the Data Retrieval Intervals

Use the Retrieval Intervals section of the TBox tab to determine how often the driver polls a TBox outstation to retrieve its point data:

To define which of the eight Normal/Promoted intervals is used for a particular point, use the Retrieval Interval field on the <Point Type> tab of the corresponding TBox Point Form (see Points Used on TBox Outstations).

Example:

An Analog Point on a TBox outstation has this configuration:
Retrieval Interval:5

The Outstation includes this configuration:
Normal Retrieval Interval 5:8S
Promoted Retrieval Interval 5:4S
The Promote when Displaying Points check box is selected.

Geo SCADA Expert scans the TBox outstation every eight seconds for the Analog Point data.

A Mimic that contains a point from the TBox outstation is displayed on one of the ViewX workstations.

While the Mimic is on display, scanning of the controller is promoted. While scanning is promoted, Geo SCADA Expert scans the TBox outstation at four-second intervals for the Analog Point data.