XAXIS Mandatory Value

The XAXIS section in a TrendSpec definition has to have one mandatory value, <X-Axis Mode>.

Mandatory Value Type XAXIS Mandatory Values
Comments

<X-Axis Mode>

Identifier value

Use to define the type of time scale used for the x-axis.

Specify one of these values:

Absolute, RelativeNow, or RelativeLatest.

(For information on each type of x-axis mode, see Configure the X-Axis.)

Example:

RelativeLatest
(For an ad hoc Trend that displays data for a time that is relative to the latest value to be plotted on the Trend.)

If required, you can specify one or more XAXIS Optional Values after the above mandatory value.