Configure the Trio Diagnostics Analog Point Properties

Use the fields on the Trio Diagnostics tab to configure an analog point’s Trio Diagnostics specific properties. Some of the fields are common to many Trio Diagnostics points (see Configure the Common Trio Diagnostics Point Properties). Fields that are specific to Simple Trio Diagnostics Analog points are explained below.