Points Used on Trio Diagnostics Radios

In the Geo SCADA Expert database, you need to configure one Simple Trio Diagnostics Point per item of diagnostics information that you want to retrieve from a Trio radio. The Simple Trio Diagnostics driver supports several types of point. Configure Trio Diagnostic points of the appropriate type to represent the type of data that you want the driver to retrieve.

The Simple Trio Diagnostics driver supports these types of point:

You configure each point that you require using the appropriate Simple Trio Diagnostics Point Form. Each Form has several tabs.

The properties on the Trio Diagnostics tab includes several driver-specific properties (see the appropriate reference above, and see Configure the Common Trio Diagnostics Point Properties).

For information on each <Point Type> tab (such as the Digital Point tab on the Simple Trio Diagnostics Digital Point Form), see the appropriate reference above.

The properties on the other tabs are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Simple Drivers).

Further Information

Create a Point and Display a Point Form: see Create and Configure a Point in the Geo SCADA Expert Guide to Core Point Configuration.