ToolTips

ToolTips provide basic help and are available for many features in Geo SCADA Expert, including List items and fields on configuration Forms. Each ToolTip contains a simple description.

To display a ToolTip, place the cursor over the item for which you require help. Do not press a mouse button. If a ToolTip exists for that item, it will appear in the form of a single-line message, displayed near the cursor.

Example:

ToolTips are available for column headings on many Lists. To display a ToolTip for a heading, place the cursor over that heading.


ToolTips are also available for fields on many configuration Forms. To display a ToolTip for a field, place the cursor over that field.