Tool Window

Tool windows display interface components that are used to configure, diagnose or navigate a Geo SCADA Expert system. These include the Explorer Bars and the Messages window.

If an interface component displays in a tool window, you can only open one instance of the component at a time.

When a tool window is displayed, you can:

When two or more tool windows are displayed, you can:

To close a tool window, either:

Or: