Display Error Reports

Associated with: WITS Device Profiles

Security permission required to access this pick action: Configure

If you use the Import Profile action and select an invalid Device Profile file, the import process will be unsuccessful. To help you identify the problems with the invalid Device Profile, Geo SCADA Expert generates an error report, which you can view by using the Display Error Reports action for a Device Profile item.

If only one error report exists for the Device Profile item, the report is displayed when you select the Display Error Reports pick action. If multiple error reports exist, a list of available reports is displayed in timestamp order. Select the report that you want to view. The report is displayed in Geo SCADA Expert.

Example:

Display Error Reports