Geo SCADA Expert User Accounts for Accessing Virtual ViewX
To use a Virtual ViewX client, users have to log on using a valid Geo SCADA Expert User Account. (The Guest User and Super User accounts are not supported by Virtual ViewX.) The User Account has to be provided with the relevant access (see Define whether a User can Access the System via ViewX, Virtual ViewX, Original WebX, or PIN via Application Code and see Define Whether any Permissions are Restricted). For more information on User Account security, see Overview of User Account Security.
The mode of operation, whether full or limited, determines whether users that have permissions to do so can make configuration changes through their web clients. For more information, see Mode of Operation of a Virtual ViewX Server.