Configure the Position of the Axis and the Color of the Axis and Trace Labels

You can specify the color and position of the x-axis. The color that you specify for the x-axis also determines the color of the label that is associated with each trace on the X-Y-Z Plot. You specify the properties using fields in the X-Axis Properties window (see Configure the X-Axis Properties).

Use the Axis section of the window to specify these properties: