Specify the Slice Fill Properties

You can specify the properties associated with a trace's slice. The 'slice' is the space between the trace's values and the start of the y-axis. You specify the slice's fill properties using fields in the Trace Properties window (see Configure a Trace).

Use the Slice Fill section of the window to specify these properties:

If a source's value drops below the minimum value that is shown on the y-axis, this will result in a 'negative' slice fill. For example, if a source's value is 0, but the y-axis range is set to a minimum of 2, this will result in a 'negative' slice that indicates the difference between the source's value of 0 and the minimum y-axis value of 2.